Electromechanical buttons on the Control Panel

Electromechanical buttons on the Control Panel

Control Panels and Panel PCs with push-button extension enable the application-specific arrangement of electromechanical buttons, switches, signal lamps, additional membrane keys and a hand wheel directly on the operating unit. The Control Panel housing is increased in size on one side. Besides the flat standard rear wall, a tray-shaped rear wall is used for the button area.

A mounting arm system can be attached to the rear wall. Depending on the mounting arm system, the cables are fed through the mounting arm. The cables for the push-button extension are fed into the mounting arm via a channel on the rear side of the Control Panel. The wiring area can be opened without having to remove the Control Panel from the mounting arm. It is possible to attach the mounting arm from below or above as desired. The housing has protection class IP 65 on all sides. The buttons, switches and signal lamps are connected to the controller via CP-Link or USB. At the same time, a second contact on the buttons and switches can be wired directly via a terminal row.

Besides the push-button extensions shown on the following pages, numerous other variants are possible, which can be individually designed in accordance with requirements.

 

Elektromechanische Taster am Control Panel
Elektromechanische Taster am Control Panel
Elektromechanische Taster am Control Panel