| Press Release | |||||||||||||||
| 16th April 2007 | |||||||||||||||
Extension of Industrial Ethernet couplers for Beckhoff I/O systems PROFINET Bus Coupler The new BK9103 Bus Coupler allows PROFINET users to use the versatile Beckhoff I/O system with more than 200 different signal types. In addition to a wide range of PROFIBUS products, Beckhoff now also supports PROFINET, the Industrial Ethernet fieldbus. The BK9103 Bus Coupler integrates the modular Bus Terminal system as a slave in the PROFINET network. The PROFINET-certified BK9103 features an integrated 2-port Ethernet Switch, which enables flexible topology configuration. For example, the I/O nodes can be configured with a line topology, instead of the traditional star topology. This reduces the wiring effort in many applications, leading to a significant reduction in installation costs. The BK9103 Bus Coupler supports PROFINET RT. It is addressed via a DIP switch meaning that the BK9103 does not require a memory card for storing the address name, and no additional configuration software is required. PROFINET is now available for additional Beckhoff product ranges. The IP 67 Fieldbus Box family supports the Industrial Ethernet version with the IL230x-B903 Coupler Box. The PROFINET device interface for the TwinCAT automation software makes the CX Embedded PCs from Beckhoff PROFINET-capable. |
|||||||||||||||
![]() |
|||||||||||||||
|
|||||||||||||||
|
|||||||||||||||