The popular TwinCAT PLC Control option of simple visualisation development is now also available as a stand-alone option. On start-up, the TwinCAT PLC HMI tool offers a full-screen display of the visualisation created with TwinCAT PLC Control. To this end, the tool only requires access to the PLC project. All visualisation features such as placeholder concept, KeyPad, NumPad, password protection, etc. can be used.
| Ordering information | |
|---|---|
| TwinCAT PLC HMI | licence for using the TwinCAT PLC HMI tool for developing visualisations under Windows NT/2000/XP/Vista |