Beckhoff at Pack Expo Las Vegas 2019

World-class performance and energy efficiency: packaging solutions with PC-based control

At Pack Expo Las Vegas 2019, Beckhoff will exhibit the next revolution in packaging technology with the eXtended Transport System (XTS). Now available in the U.S., the XTS implements flexible changeovers in seconds with less required components. At the same time, the exciting mechatronic solution minimizes machine footprint and reduces raw material and energy consumption.

Further trailblazing innovations – from IoT to advanced motion control – await you at booth LS-6149 in the lower south hall.

Beckhoff is also excited to offer you complimentary registration to Pack Expo Las Vegas! To register, simply click here and follow the registration prompts. During the registration process, enter: 59D15 in the box labeled “comp code,” and the $30 registration fee will be waived. The Beckhoff team is looking forward to your visit!

Innovation Stage Presentation (Booth C-1049)

Want a deeper look into the technology behind XTS? Beckhoff will also present the latest updates on this groundbreaking mechatronic technology for packaging applications at the Pack Expo Las Vegas Innovation Stage! On Tuesday of the show, be sure to attend: “Faster, smaller, smarter: Drive technology advances power next gen packaging.”

Tuesday, September 24 | 11:00 a.m. | Innovation Stage | Booth C-1049

More information

Highly efficient packaging of toothbrushes
Cosmetics filling line for up to 100 container formats

Packaging optimization through TwinCAT Vision

Packaging optimization through TwinCAT Vision

TwinCAT Vision will make its North American debut at Pack Expo 2019. With this system-integrated vision platform, Beckhoff adds image processing capabilities directly into the packaging machine controller. Track-and-trace, high-precision measurement and precise visual inspection increase efficiency and quality in packaging and production.

TwinCAT Vision

Reduced packaging machine footprint with the AMP8000

Reduced packaging machine footprint with the AMP8000

The AMP8000 servomotor with integrated servo drive minimizes control cabinet requirements and machine footprint. This innovative design saves material, space, costs and assembly work in motion control systems.

AMP8000

Ultra-compact Industrial PCs: high-end computing power in a space-saving design

The Industrial PC series that started with the C6015 has proven itself through its low space requirements, universal usability and flexible mounting. The C6017 offers additional interfaces and an integrated UPS. The C6030 was developed for applications with maximum power requirements. Apart from the well-known benefits, the PC features maximum computing power: the multi-core computer integrates Intel® Core™ i processors of the 6th and 7th generation and offers top performance with up to 3.6 GHz per core with 4 cores. Beckhoff has further developed the Industrial PC series with the new C6032, which offers additional interfaces compared to the C6030.

Ultra-compact Industrial PCs

Ultra-compact Industrial PCs: high-end computing power in a space-saving design

Show information

Las Vegas, NV, USA
September 23 – 25, 2019
Hall: Lower South
Booth: 6149

Site Plan Pack Expo

Pack Expo Las Vegas 2019

Main information

Beckhoff booth:

  • Hall: Lower South
    Booth: 6149

Opening hours:

  • Daily
    9:00 a.m. – 4:00 p.m.