Aug 17, 2018

MATLAB®/Simulink® integration: XTS pendulum showcase

MATLAB®/Simulink® integration: XTS pendulum showcase

MATLAB®/Simulink® modules from The MathWorks are perfect supplements to hardware and software components from Beckhoff Automation.

More about this video

TE1400 | TwinCAT 3 Target for Simulink®

TE1400

TwinCAT 3 Target for Simulink® provides an interface between Simulink® and TwinCAT. The Simulink® software is developed and distributed by the MathWorks company. The programming environment is based on MATLAB® and is widely used both in science and in industry. Simulink® is a graphic programming environment that is ideally suited to the model-based development process. Simulation models of systems can be created and, for example, control and feedback control algorithms in order to test the models created.

TE1410 | TwinCAT 3 Interface for MATLAB®/Simulink®

TE1410

MATLAB® and Simulink® are developed and distributed by the MathWorks company. The two programming environments are widely used both in science and in industry. Simulink® is a graphic programming environment that is ideally suited to the model-based development process. MATLAB® is a script language for the development of algorithms and mathematical models.

TwinCAT

The TwinCAT software system turns almost any PC-based system into a real-time control with multiple PLC, NC, CNC and/or robotics runtime systems.

XTS | Linear product transport

As an intelligent transport system, the eXtended Transport System enables flexible motion profiles and new types of machine concept.