Apr 17, 2019

Hannover Messe 2019

XPlanar: Motion Revolution

The XPlanar stands for a revolution in motion control: maximum flexibility, long living, energy-efficient

More about this video

XPlanar

Highly compact and fully integrated drive unit that allows any product to be lifted.

APM4220-0000-0000

The APM4220-0000 XPlanar mover is the smallest mover in the APM4xxx family and is compatible with all tiles of the type APS4xxx. With a payload of up to 400 g, the mover is ideal for handling small, lightweight products with a high packing density.

APM4330-0000-0000

The APM4330-0000 XPlanar mover is the all-rounder of the APM4xxx family and is compatible with all tiles of the type APS4xxx. With a load capacity of up to 1.5 kg, the mover is ideally suited for use as a universal tool for handling different products in all industries. Even more elaborate workpiece carriers and attached parts can be used to implement the individual requirements.

APM4550-0000-0000

The APM4550-0000 XPlanar mover is the strongest member of the APM4xxx family and is compatible with all tiles of the type APS4xxx. With a load capacity of up to 4.2 kg, the mover is suitable for the handling of larger and heavier products. Even more elaborate workpiece carriers and attached parts can be used to implement the individual requirements.

APS4322-0000-0000

The APS4322-0000 XPlanar tile is the basic building block of the XPlanar system. All movers of the type APM4xxx can be operated on this tile. Depending on the mover size, bi-directional or unidirectional operation on a tile is possible. Multiple movers can also be operated on the tile at the same time. Like all XPlanar tiles, the APS4322-0000 is a fully integrated drive and can be flexibly arranged and covered. Additional infrastructure components such as power supply units or port multipliers are no longer required.

APS900x

The XPlanar starter kits are complete XPlanar systems for a quick entry into the non-contact product handling of tomorrow. In order to conserve valuable development resources, the starter kits are delivered fully assembled and tested. They include the tiles, the machine bed, the movers and the Industrial PC as well as a software example. After opening the transport box, the user can immediately commence with the first tests.