הפרדהתיקוןסגירה

Dec 1, 2022

Using high-end multi-touch panel PCs directly in the field

Multi-touch can be implemented directly in the field in high-end panel PCs from the CP32xx series. These devices, housed in robust aluminum, feature complete IP65 protection and are designed for mounting arm installation. This video shows you more features of the CP32xx-1600.