Beckhoff Control Panels with modern multi-touch technology
Beckhoff Multitouch Control Panels combine Moultitouch and other technologies from the consumer goods market with the requirements for robust and durable control units.
More about this video

CP29xx, CP39xx | Multi-touch Control Panels
The Control Panel series CP29xx and CP39xx in diagonals from 7 to 24 inches offer modern multi-touch technology and flexible connection technology for distances of up to 100 meters.

CPX29xx, CPX39xx | Ex Control Panels
The Control Panel series CPX29xx and CPX39xx offer multi-touch technology for distances of up to 100 meters for use in Zone 2/22.

CP29xx | Multi-touch built-in Control Panel
Balance between latest PC technology and long-term availability of control components
Modern Control Panel technology doesn't stop with the selection of the touch technology, which forms the basis of the operation of a machine or plant. The transmission of the image and touch signals, combined with the power supply or other digital signals, must work perfectly and continuously, both mechanically and electrically, and over long distances in the industrial environment. In order to reliably ensure this, Beckhoff installs Panel electronics that it develops and manufactures itself at the production location in Verl.

CP39xx | Multi-touch Control Panel
Balance between latest PC technology and long-term availability of control components
Modern Control Panel technology doesn't stop with the selection of the touch technology, which forms the basis of the operation of a machine or plant. The transmission of the image and touch signals, combined with the power supply or other digital signals, must work perfectly and continuously, both mechanically and electrically, and over long distances in the industrial environment. In order to reliably ensure this, Beckhoff installs Panel electronics that it develops and manufactures itself at the production location in Verl.

CP29xx-0000 | Multi-touch built-in Control Panel with DVI/USB Extended interface