At ISE 2022, which will take place from May 10 to 13 in Barcelona, Beckhoff will demonstrate how open automation solutions can open up new possibilities in AV and media technology. Beckhoff is thereby focusing on new solutions for audio and video system integration and on its own competence as an automation partner.
A prime example is the cooperation with AV Stumpfl and its PIXERA system. System integrators now have the option of easily integrating the components of open PC- and EtherCAT-based control technology from Beckhoff into the PIXERA system. This is made possible by PIXERA control, the new software-based integration and control framework. The coordinated hardware packages can be interconnected with one another using a convenient plug-and-control function.
Beckhoff will also be showing other current highlights for media and entertainment technology: On the one hand, the DIN rail-mountable embedded PCs of the CX5600 series with AMD Ryzen™ processors, which are characterized by low power consumption and fanless operation, and on the other hand, the EL2564 digital output terminal for cost-effective control of LEDs with integrated series resistor via an adjustable (ground-switching) PWM signal.
Industries

Mr. Volkan Yücel
Beckhoff Otomasyon ltd. şti.
Gardenya-3 Plaza No: 18-19-20
34758 Istanbul
Türkiye
+90 532 111 4 225
press@beckhoff.com.tr
www.beckhoff.com/tr-tr/