AyırSabitleKapat

Ultra-compact Industrial PC series expanded by device with Intel® Core™ i U processor

C6025: Intel® Core™ i computing power in a highly compact, fanless design

The ultra-compact Beckhoff C6025 Industrial PC is designed to deliver the high computing performance of the Intel® Core™ i series in a fanless, small-form-factor device. The new Intel® Core™ i U processors, with exceptionally low power requirements, have made this possible.

Measuring just 82 x 127 x 40 mm and combining high computing performance with a fanless design, the new C6025 IPC is an ideal choice for demanding control applications where green, sustainable IT is also a requirement. It is built around the Intel® Core™ i U processors that deliver Core™ i performance capabilities yet consume significantly less power than other processors of the same series. The 8th Gen Intel® Core™ i U processors used in the C6025 also offer an advantage which is typical of evolving PC technology: higher performance at the same price point. With this new addition, the Beckhoff portfolio of industry-ready and long-term available Industrial PCs now spans five CPU performance classes – from ARM through to Intel® Xeon® – for maximum scalability.

The IPC’s energy-efficient Intel® Core™ i U processors, in combination with an advanced cooling design, enable fully passive heat dissipation via a heat sink on one side. Housed in an aluminum and zinc die-cast enclosure, the C6025 offers a feature set that includes the following:

  • up to four CPU cores
  • 4 GB DDR4 RAM (expandable to 8 GB)
  • 40 GB M.2 SSD with 3D flash memory
  • 1 x DisplayPort video connector
  • 4 x USB 3.0 ports
  • on-board Ethernet controller with 3 x 100/1000Base-T ports
  • operating temperature range of 0 to 50° C

The power-efficient, ultra-compact C6025 Industrial PC expands the broad IPC portfolio from Beckhoff with a device that offers a performance level situated between the entry-level devices with Intel Atom® CPUs and those with high-performance Intel® Core™ i-series processors. With this addition, the product portfolio better addresses the growing trend toward compact, fanless Industrial PCs while supporting applications with highly intensive computing requirements.

Mr. Volkan Yücel

Mr. Volkan Yücel
Beckhoff Otomasyon ltd. şti.
Gardenya-3 Plaza No: 18-19-20
34758 Istanbul
Türkiye

+90 532 111 4 225
press@beckhoff.com.tr
www.beckhoff.com/tr-tr/