Press Release

6th April 2008

TwinCAT Building Automation Framework

Configuring instead of programming

“Configuring instead of programming” is the motto of the TwinCAT Building Automation Framework. This approach markedly simplifies engineering and commissioning and does not call for any programming expertise. It enables system integrators, operators and building users to quickly and easily incorporate new functions, modify scenarios or re-assign sensors and actuators – all with just a few clicks.

Beckhoff Building Automation offers two ways of setting up and commissioning building projects. Complex projects are programmed using TwinCAT PLC automation software, which conforms to international IEC 61131 3 programming standards. There are already comprehensive PLC libraries available for TwinCAT PLC, for example for HVAC, lighting systems or for integrating subsystems such as EIB or LON.

The new TwinCAT Building Automation Framework offers an alternative approach to supporting system integrators engaged in developing and commissioning such applications. The Building Automation Framework incorporates the Building Automation Manager and the application program. The Building Automation Manager is the system’s configuration control centre. This is where the available components, such as Industrial PCs, Embedded PCs, Bus Terminals and data points are entered and assigned to the appropriate functions.

The status of all the system’s sensors and actuators can be viewed and controlled via the TwinCAT Building Automation Manager. The actuators can also be triggered by hand – for instance when the system is being commissioned. Configuration wizards are also provided to enable users to easily link actuators and sensors.



Press picture
TwinCAT Building Automation Framework
Picture caption:
Engineering and commissioning building projects are markedly simplified by the TwinCAT Building Automation Framework. Users can rapidly modify scenarios or change the assignments of sensors and actuators.
 

Download:
Presskit (ZIP file)


Further informations:
TwinCAT
TwinCAT Building Automation Framework
Press releases


Back Top Beckhoff Press contact