| Microsoft launch of Windows Embedded CE 6.0 R2 in Japan |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1,9 MB |
| Date: |
27.11.2007 |
Download pr332007.zip |
Microsoft launch of Windows Embedded CE 6.0 R2 in Japan. The operating system recognises connected Ethernet devices automatically via the Web Services on Devices technology and integrates them in the overall system. |
 |
| CU2508 port multiplier |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2,9 MB |
| Date: |
27.11.2007 |
Download pr322007.zip |
The CU2508 port multiplier with multi-protocol capability can operate up to eight independent real-time Ethernet networks on one PC. |
 |
| EK1501 EtherCAT Coupler |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
3,2 MB |
| Date: |
27.11.2007 |
Download pr312007.zip |
EtherCAT via fibre-optic technology: Using the EK1501 EtherCAT Coupler and/or the EK1521 junction terminal, more flexible topologies are now possible with glass fibre technology. |
 |
| EtherCAT Terminals for XFC |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2,66 MB |
| Date: |
27.11.2007 |
Download pr292007.zip |
The EtherCAT terminal product range covers a wide range of different I/O terminals and special versions for the time stamp, oversampling and fast I/O XFC technologies. |
 |
| Ethernet controller |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2,43 MB |
| Date: |
27.11.2007 |
Download pr282007.zip |
All Ethernet controllers offer a wide range of application options, including industrial automation and intelligent building services. |
 |
| Embedded PC CX1010 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1,65 MB |
| Date: |
27.11.2007 |
Download pr272007.zip |
Beckhoff Bus Terminals and EtherCAT Terminals can be connected directly to the CX1010 Embedded PC via different power supply units. |
 |
| Beckhoff creates Chinese subsidiary |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2,84 MB |
| Date: |
27.11.2007 |
Download pr262007.zip |
Kai Ristau, International Sales Manager of Beckhoff Automation GmbH. |
 |
| EK9750 Bus Coupler |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2,9 MB |
| Date: |
05.10.2007 |
Download pr232007.zip |
With the EK9750 Bus Coupler, the powerful and ultra-fast Beckhoff I/O system is available for SERCOS III networks. |
 |
| Industrial Motherboard CB4051 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2636 kB |
| Date: |
27.09.2007 |
Download pr222007.zip |
New high-technical Industrial Motherboard CB4051 from Beckhoff with a powerful Intel® 945GM(E) chipset and Intel® Core™ Duo or Intel® Core™2 Duo processors. |
 |
| Embedded PC CX9010 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
3446 kB |
| Date: |
27.09.2007 |
Download pr212007.zip |
The Beckhoff Embedded PC CX9010 is equipped with an Intel® IXP420 processor with XScale® technology. |
 |
| AM3500 servomotors |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2214 kB |
| Date: |
17.09.2007 |
Download pr202007.zip |
Against the trend: The AM3500 servomotors from Beckhoff have a higher moment of inertia, making them particularly suitable for machine tool axes with stringent synchronism requirements or applications with higher inertia. |
 |
| PC-based control technology |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2918 kB |
| Date: |
07.09.2007 |
Download pr192007.zip |
Beckhoff presents its solution for the PC-based control technology at K 2007 in Düsseldorf, Germany: The main focus is on EtherCAT-based automation, XFC and the Beckhoff Drive Technology. |
 |
| CP6608 Ethernet Control Panel |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2270 kB |
| Date: |
31.08.2007 |
Download pr182007_1.zip |
The CP6608 Ethernet Control Panel features an integrated PC and is ideal for a wide range of industrial automation applications. The panel can be used as a pure touch screen panel or as an “all-in-one” PC controller. |
 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
2286 kB |
| Date: |
31.08.2007 |
Download pr182007_2.zip |
 |
| Jitendrakumar Kataria, managing director of Beckhoff Automation Pvt. Ltd. |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1505 kB |
| Date: |
31.08.2007 |
Download pr172007.zip |
Jitendrakumar Kataria, managing director of Beckhoff Automation Pvt. Ltd., has lived in Germany for the last 5 ½ years and has worked for more than four years in the development department at Beckhoff in Verl, Germany. He has excellent specialist knowledge in the area of automation and is familiar with both the Indian and European markets. |
 |
| EtherNet/IP for Fieldbus Box modules |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
3106 kB |
| Date: |
02.08.2007 |
Download pr162007.zip |
The compact and robust Fieldbus Box modules act as decentralised I/Os directly at the machine or system and are now also available for EtherNet/IP. |
 |
| New control concept for metalworking |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
3178 kB |
| Date: |
02.08.2007 |
Download pr142007.zip |
The new generation of Beckhoff with PC and EtherCAT-based control technology. |
 |
| PC-based Control for the wood industry |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
3805 kB |
| Date: |
14.05.2007 |
Download pr132007.zip |
Open automation solutions for the wood industry. |
 |
| XFC: eXtreme Fast Control Technology |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1335 kB |
| Date: |
16.04.2007 |
Download pr122007.zip |
The I/O response time includes all hardware processing times (IPC, EtherCAT and I/O system), ranging from physical input event to output response. |
 |
| Industrial Motherboards |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1900 kB |
| Date: |
16.04.2007 |
Download pr102007.zip |
3.5" Industrial Motherboard from Beckhoff. |
 |
| Embedded PC CX1030 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1399 kB |
| Date: |
16.04.2007 |
Download pr092007.zip |
The Beckhoff Embedded PC CX1030 is equipped with a 1.8 GHz Intel® Pentium® M. |
 |
| Multichannel probe ET2000 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
853 kB |
| Date: |
16.04.2007 |
Download pr082007.zip |
Multichannel probe ET2000 for analysing Industrial Ethernet solutions. |
 |
| Control Panel CP79xx |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1469 kB |
| Date: |
16.04.2007 |
Download pr072007.zip |
Via the DVI/USB Extended interface the CP79xx Control Panels can be installed at a distance of up to 50 m from the PC as standard. |
 |
| TwinCAT and Industrial PCs support Core™ Duo processors |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1992 kB |
| Date: |
16.04.2007 |
Download pr062007.zip |
The PC-based control technology from Beckhoff supports the multi-core architecture of Intel® Core™ Duo processors. |
 |
| PROFINET Bus Coupler BK9103 |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1442 kB |
| Date: |
16.04.2007 |
Download pr052007.zip |
The BK9103 PROFINET Bus Coupler complements the product range of the Beckhoff Bus Terminal system. |
 |
| CP72xx "Economy" Panel PC |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1025 kB |
| Date: |
15.03.2007 |
Download pr042007.zip |
The CP72xx "Economy" Panel PC from Beckhoff with compact slimline housing meets all requirements for advanced machine control. |
 |
| Industrial PC solutions score in industrial IT environments |
 |
Press release
| Format: |
JPG, zip-compressed |
| Size: |
1180 kB |
| Date: |
15.03.2007 |
Download pr032007.zip |
Beckhoff IPC technology is ideally suited for industrial IT applications. |
 |
| Beckhoff takes full advantage of new Embedded operating system from Microsoft |
 |
Presse release
| Format: |
JPG, zip-compressed |
| Size: |
1836 kB |
| Date: |
13.02.2007 |
Download pr022007.zip |
With the Embedded PC and Panel PC product range Beckhoff takes full advantage of the Windows Embedded CE 6.0 operating systems from Microsoft. |
 |
| Beckhoff PC Fieldbus Cards with Mini PCI interface |
 |
Presse release
| Format: |
JPG, zip-compressed |
| Size: |
1491 kB |
| Date: |
13.02.2007 |
Download pr012007.zip |
Beckhoff Mini PCI cards take fieldbus functionality in a compact way into the IPC. |
 |