Sídlo Česká republika
Beckhoff Automation s.r.o.

Sochorova 23
61600 Brno, Česká republika

+420 511 189 250
info.cz@beckhoff.com
www.beckhoff.com/cs-cz/

Sep 1, 2020

ETG officially supports EtherCAT G

ETG Technical Committee accepts technology addition

The Technical Committee of the EtherCAT Technology Group (ETG) has accepted EtherCAT G as an addition to the EtherCAT standard. Moving forward, EtherCAT G, which extends EtherCAT technology to 1 and 10 Gbit/s, respectively, will be supported and promoted by the ETG.

Currently, the ETG is working to add EtherCAT G to the corresponding technology specifications. Dr. Guido Beckmann, Chairman of the ETG Technical Committee, explains why ETG welcomes the active integration of EtherCAT G into ETG: “EtherCAT is already the fastest industrial Ethernet fieldbus, and will remain so due to its special functional principle. With EtherCAT G, particularly data-hungry applications, such as machine vision and high-end measurement technology, can now also be integrated. This extends the range of applications for EtherCAT technology and makes it even more viable for the future.”

The well-known 100 Mbit/s EtherCAT technology remains the proven solution for the majority of applications. However, EtherCAT G offers additional user advantages, especially in applications where particularly large amounts of process data must be transported per device. This can include, e.g., machine vision, high-end measurement technology or complex motion applications that go beyond the scope of classic drive control. As an extension of standard EtherCAT technology, EtherCAT G is fully compatible; existing devices designed for 100 Mbit/s can be seamlessly integrated into an EtherCAT G system, and EtherCAT G devices in a 100 Mbit/s EtherCAT system behave like classic EtherCAT devices.

The central element of EtherCAT G is the use of EtherCAT Branch Controllers, which essentially fulfil two main functions: On the one hand, they act as a kind of node for the integration of segments from 100 Mbit/s devices; on the other hand, they enable parallel processing of the connected EtherCAT segments. This significantly reduces the propagation delay in the system, which increases system performance many times over previous levels.

Typical for EtherCAT: The integration of EtherCAT G is simple, as the extension is fully compatible with the IEEE 802.3 Ethernet standard and no software adaptations in controllers are required for the standard mode. “The advantages of EtherCAT are well known and include processing on the fly, comprehensive diagnostics, simple configuration and integrated synchronization,” says Beckmann. “These attributes are of course fully retained when EtherCAT G is used.”