Sep 15, 2022

Innovative automation concepts for media and building technology

Beckhoff – in cooperation with the Austrian projection specialists from AV Stumpfl – presents the integration of Beckhoff hardware in the software-based PIXERA control framework.

System integrators now have the option of easily integrating the components of open PC- and EtherCAT-based control technology from Beckhoff into the PIXERA system. This is made possible by PIXERA control, the new software-based integration and control framework. The coordinated hardware packages can be interconnected with one another using a convenient plug-and-control function.

Further information