TwinCAT HMI | The next HMI generation
What does the HMI solution of the future look like? How can the all-important user interface be given an industry-spanning design in the future so that maximum operator efficiency and optimum user comfort are ensured?
In this 30-minute webinar Sven Oberschmidt, TwinCAT Product Manager, will introduce with TwinCAT HMI the next HMI generation. TwinCAT now integrates the Human Machine Interface directly into the familiar environment of Microsoft Visual Studio®. Programming is unnecessary as configuration is handled with ease using the TwinCAT HMI graphical editor. This web-based solution, which is based on HTML5, acts “responsively”, irrespective of the operating system, browser and device.
More about this video
TE2000 | TwinCAT 3 HMI Engineering
The TwinCAT 3 HMI (human-machine interface) integrates itself into the well-known Visual Studio® development environment. Based on the latest web technologies (HTML5, JavaScript), it allows the user to develop platform-independent user interfaces that are responsive, i.e. they automatically adapt to the screen resolution, size and orientation at hand. With the graphical WYSIWYG (what-you-see-is-what-you-get) editor, controls can be easily arranged via drag-and-drop and linked with real-time variables.
TF2000 | TwinCAT 3 HMI Server
The TwinCAT 3 HMI Server is a modular web server that provides the human-machine interface (HMI). It supports all CPU classes from