Learn how to set up the simulation runtime in TwinCAT and how to generate the FMU. This can then be used in an arbitrary FMI-Importer Tool for simulation.
More about this video
Software (Automation)
Software TwinCAT nabízí mnoho funkcí a širokou škálu softwarových modulů pro všechny úlohy automatizace.
TExxxx | TwinCAT 3 Engineering
The TwinCAT 3 engineering components enable the configuration, programming and debugging of applications.
TE1421 | TwinCAT 3 Simulation Runtime for FMI
The TwinCAT 3 Simulation Runtime for FMI provides an interface for simulation tools that support the Functional Mockup Interface (FMI). The interface is based on the TwinCAT 3 UserMode Runtime, which can be accessed in sync from the simulation tool. This is exported to an FMU together with an interface description configured in TwinCAT, and can be imported into any simulation tool that supports the FMI interface as a co-simulation. Support is offered for both FMI 2.0 and 3.0. The TwinCAT project that is being executed in the FMU can also be part of the FMU; however, it is also possible to connect to this UM runtime with a TwinCAT engineering system and monitor or modify the code executed in the FMU in TwinCAT.