Multi-touch can be implemented directly in the field in high-end panel PCs from the CP32xx series. These devices, housed in robust aluminum, feature complete IP65 protection and are designed for mounting arm installation. This video shows you more features of the CP32xx-1600.
More about this video
CP32xx | Multi-touch Panel PC
With the CP32xx series, a high-end Panel PC with multi-touch can be used directly in the field. The devices in a slender aluminum housing feature complete IP65 protection and are designed for mounting arm installation. The Panel PCs offer maximum computing power with processors of the latest generation, such as Intel® Celeron®, Intel® Pentium® or Intel® Core™ i3/i5/i7.
CP32xx-1600 | Multi-touch Panel PC
Multi-touch can be used directly in the field with the CP32xx-1600 Panel PC series. The devices in robust aluminum housing feature complete IP65 protection and are designed for mounting arm installation. The Panel PCs offer maximum computing power with processors of the latest generation, such as Intel® Celeron®, Pentium® or Core™ i3/i5/i7. There is a choice of six different multi-touch TFT displays from 15 to 24 inches, in the formats 4:3, 5:4 and widescreen 16:9. An optional C9900-G05x push-button extension can be ordered ex factory.