Oct 8, 2026

Precision at Production Speed

High-Speed Die Sorting for the Smallest Semiconductor Components Imaginable

In the wake of semiconductor reshoring to the United States, the winning die sorting line is the one that can quickly scale from high-mix research and development to production-level volumes without sacrificing precision. As wafer processing ramps up domestically, manufacturers need equipment that can sort fragile dies at high speed, verify quality inline, and reconfigure quickly for different sizes and packaging formats. V-TEK’s Royce Instruments brand answered that call with the High-Speed Sorter, a new production-oriented system capable of micron-level accuracy, gentle handling, and first-pass yields with dramatically higher throughput than its predecessor.

Based in Mankato, Minnesota, V-TEK and Royce Instruments have delivered specialty systems for die sorting, bond testing, and ultra-small-part handling for more than 40 years. Both brands were founded in the mid-1980s, and V-TEK acquired Royce in 2014. “For decades, we’ve specialized in high-mix, low-volume semiconductor applications,” says Matt Wilson, Vice President of Sales at V-TEK Inc. “Now, with U.S. production ramping up, customers need the same precision, but at production scale. The High-Speed Sorter (HSS) is our answer.”

V-TEK Royce Instruments High-Speed Sorter.
The V-TEK Royce Instruments High-Speed Sorter delivers production-grade die sorting with micron-level precision and throughput up to 5,000 parts per hour.

Precision under pressure

Balancing speed and gentle handling is the central challenge in modern die sorting. Dies are smaller and more delicate, and even subtle mishandling during ejection, pickup, inversion, or placement can quickly degrade yield. The motion control system must deliver repeatable, micron-level positions, and the axes must move in tight coordination through complex profiles. At the same time, manufacturers want to add inline quality checks, defect inspection, and electrical testing, while parts are already singulated, without slowing down the line or adding additional handling.

“Some of the important aspects are related to accuracy and precision,” Wilson explains. “Our systems have to be highly precise, into the micron type level, and also very gentle at the same time so that we’re not damaging fragile customer components.”

Flexibility is just as critical. Production lines must change over among different die sizes and multiple output formats, including carrier tape, waffle packs, and gel packs. Changeover time should be measured in minutes rather than hours. Cleanroom compliance imposes further constraints on components and lubricants, and CE emissions rules affect even basic details, such as display connections outside the control cabinet. The control architecture must be open and modular to adapt quickly as the product matures, and customers request late-stage changes.

“One of the big challenges is keeping the system flexible so it can run different part sizes with minimal changeover time,” adds Matthew Werner, Applications Engineer at V-TEK Inc. “While we must run really small parts, we also must be able to handle larger parts as well. Many of the parts we deal with are very fragile, so we need to handle them carefully but also quickly to ensure that the system delivers the high throughput we want in the field.”

Sorting out the future

After evaluating multiple control platforms, V-TEK selected Beckhoff’s PC-based automation platform with EtherCAT networking and TwinCAT software. This choice was influenced by Beckhoff’s confidence in meeting the project’s complex requirements, direct engineering support, and a technology stack capable of coordinating dozens of axes, integrating safety, and remaining open to future machine vision integration.

“Beckhoff’s confidence in their product convinced us from the start,” says Scott Miller, Engineering Manager at V-TEK Inc. “Every challenge we threw at them was met with a response of, ‘That’s not a problem,’ and they proved it.”

Closeup of V-TEK Royce Instruments High-Speed Sorter.
Beckhoff-driven motion technology helps protect delicate components through every stage of the sorting process.

The HSS is built around Beckhoff’s unified control architecture. TwinCAT 3 serves as the single engineering environment for PLC and motion, leveraging object-oriented programming (OOP) for easier code reusability, modularity, and debugging. “I like TwinCAT 3's incorporation of object-oriented architectures. It has made a system with so many axes a lot easier to use because we can define the common class between all the axes,” says Alex Lloyd, Controls Engineer at V-TEK.

A C6032 ultra-compact Industrial PC runs PLC, motion control, and HMI in one device, with DisplayPort video output aiding CE compliance by reducing noise. EtherCAT provides deterministic, straightforward networking across drives, I/O, and safety devices, eliminating the complexity of managed switches, IP addresses, and multicast settings encountered in previous projects networked via EtherNet/IP. “EtherCAT has been easier to work with. In the past, some of the EtherNet/IP implementations I used weren’t very intuitive, but the EtherCAT devices we’ve used have been intuitive and easy to set up,” Floyd notes.

The motion hardware includes EL7212 servo terminals and EL70xx stepper terminals, integrating the drive and control into compact DIN rail-mounted I/O modules. This reduces hardware footprint and wiring compared to traditional standalone drives. “Previously with steppers, we had to have a module for the PLC and then the driver as well. With the Beckhoff stepper terminals, it’s all-in-one. It eliminates a piece of hardware, and it’s smaller than either of those components individually,” Floyd explains. AX8000 multi-axis servo drives deliver high-performance motion, including the AX8108 drive, which can handle dual encoders and custom rotary motors with extremely high-tick-counts. “Fortunately for us, Beckhoff was in the process of rolling out a new drive; they were able to get our hands on one in a month or two. It worked well out of the box,” Miller recalls. AM8000 servomotors with One Cable Technology (OCT) simplify installation and cabinet routing.

Coordinated eject-and-pick profiles are essential for fragile die handling. Eject needles and pickup tips move in synchrony to lift dies cleanly, avoiding micro-damage and preserving yield. With TwinCAT, V-TEK synchronized axis dynamics to achieve reliable, repeatable motion sequences for ejection, inversion, and placement.

The HSS was designed with late-stage changes in mind. By reserving DIN-rail space for snap-on expansions and EtherCAT’s networking capacity for up to 65,535 devices, adding an axis often means simply adding a terminal and updating software rather than rearchitecting panels. “Compared to the prior generation system, which used banks of standalone stepper drives requiring thermal spacing and cross-panel wiring, the Beckhoff drives cut installation time, wiring, and panel area significantly,” said Miller.

Operator using V-TEK Royce Instruments High-Speed Sorter.
Built on Beckhoff PC-based control and EtherCAT networking, the High-Speed Sorter achieves a fivefold increase in throughput over previous generations.

Cleanroom considerations influenced the design from the start. The final architecture retained precision, modularity, and serviceability while mitigating contamination risk, helping keep the HSS aligned with cleanroom best practices.

TwinCAT 3’s integration with Visual Studio lets V-TEK house PLC, motion, and HMI in a single solution, applying standard software practices such as modular libraries, reuse, and version control to a complex mechatronic machine. It also permits programming in C#, Structured Text, and Object-Oriented Programming in one environment. TwinCAT 3 and the multi-core C6032 IPCs enable heavy duty tasks to be isolated to individual cores. On certain systems, for example, cores are dedicated to camera processing while additional cores handle motion control and other functions. EtherCAT’s built-in diagnostics allow the team to quickly localize and correct cabling issues, reducing troubleshooting time from days to minutes.

Support from Beckhoff’s local engineering team in Minnesota also played a role. “Direct access to product specialists helped the V-TEK team validate concepts, tune performance, and resolve issues on compressed timelines,” says Miller. “That’s been pivotal.”

The speed of success

The High-Speed Sorter met its most important goal immediately. On representative small devices, the HSS achieved 5,000 parts per hour on 2 × 2-millimeter dies—five times faster than the AP Plus generation it replaces. “We hit our throughput goal right out of the gate, and that was our target from day one,” Wilson says. “When we defined the scope of the HSS project, that throughput number has been there from the beginning. To immediately solve that challenge was very exciting.”

Perhaps most importantly, the platform is built to adapt. Inline electrical test and vision inspection can be added while parts are already singulated, delivering value without excessive handling. Outputs can be configured for carrier tape, waffle packs, or gel packs without major mechanical rework. Those late-stage customer changes, common as users explore capabilities during acceptance testing, are absorbed more gracefully through EtherCAT’s modularity and the reserved cabinet capacity.

AX8620 power supply module inside control cabinet.
The AX8620 power supply module delivers the power foundation needed to coordinate the High-Speed Sorter's demanding multi-axis motion applications.

The HSS program also catalyzed modernization across V-TEK’s entire portfolio of equipment. The DE-35 bond tester now ships with Beckhoff controls; the team worked with Beckhoff to deliver required performance without upsizing the controller, protecting cost targets. The forthcoming Royce 600-series bond tester is also being developed on a Beckhoff architecture, with the company’s planned first use of Beckhoff Vision to enable vision-guided motion on a bond tester. Beyond Royce-branded systems, V-TEK is evaluating further system migrations to Beckhoff as obsolescence pressures rise, and customers ask for greater flexibility at competitive cost.

“The most impactful transformations occur when customers are willing to challenge the status quo,” says Cody Dirksen, Sales Engineer at Beckhoff USA. “Through close collaboration across engineering, product, and business teams, beta technology became the catalyst for innovation at V-TEK. The Beckhoff solution delivered the speed and flexibility required to revolutionize an entire system.”

The aggressive development timeline underscores the pace at which the semiconductor industry can move. Concept and vendor selection began in early 2024. Builds started in early 2025, followed by first testing mid-year. The HSS publicly debuted at the SEMICON West trade show in October 2025, where Beckhoff support helped ensure reliable operation of the new system on the show floor.

The High-Speed Sorter marks a decisive step toward production-grade capabilities for V-TEK and Royce Instruments without compromising the quality and precision their customers expect. By unifying motion, logic, and safety on Beckhoff’s PC-based control platform with EtherCAT networking, V-TEK’s Royce Instruments team delivered a production-ready die sorter that maintains the brand’s hallmark precision while achieving a five-fold leap in throughput on incredibly small components. The close engineering collaboration between V-TEK and Beckhoff helped ensure that the High-Speed Sorter can meet the demands of a reshored and rapidly changing semiconductor manufacturing landscape.

Further information