Oficina central México
Beckhoff Automation, S.A. de C.V.

Boulevard Manuel Ávila Camacho 2610, Torre B, Piso 9, Colonia Valle de los Pinos, Tlalnepantla de Baz
Estado de México CP 54040, México

+52 55 75998058
mexico@beckhoff.com
www.beckhoff.com/es-mx/

Sep 7, 2026

Stage technology: Retrofit without altering the mechanics

Integrated PC-based control ensures unlimited, simplified, and fluid movements

With a blend of classical, traditional, and contemporary styles, the “Racines” production at the Opéra Bastille offers a multifaceted immersion into the world of dance. Not only has the performances’ choreography been constantly adapted to the movements of the dancers, but there have also been consistent efforts to incorporate the stage design. With the help of Beckhoff automation technology, the background movements are synchronized with those of the dancers and formed into sophisticated blends of stagecraft.

The Opéra national de Paris – with its two major venues, the Palais Garnier and Opéra Bastille – is known far beyond France and Europe as a whole for the quality and diversity of its programming. Its aim is to make the world’s heritage of lyrical and choreographic works accessible to as many people as possible – and, with more than 400 performances per year and a total audience of around 900,000, this is something it achieves very well. Its success requires significant amounts of technical work and expertise: Ultimately, the magic seen on the stage is created not only by the teamwork between the dancers, choreographers, directors, and musicians, but also in large part by the craftspeople and technicians behind the scenes. There are five stage engineers at the Palais Garnier and 20 at the Opéra Bastille. Sébastien Fournier, Deputy Head Of Stage Technology at the Opéra Bastille, explains how they view their role: “Our job includes anticipating the technical requirements of the production. In order to do justice to the creative spirit of the directors and create unique moments for visitors, we need a technical foundation that sets as few limits as possible. That’s where PC-based control from Beckhoff makes a huge difference.”

Two dancers dressed in black perform against a backdrop of red streaks of light on a dark stage.
Just as musicians follow a score, the mechanical units in the stage design, known as patiences, also execute different movements.

Movement at the heart of the production

In “Racines”, screens accompany the dancers’ movements, creating a production that is fluid and intricate at the same time. “The solution that Beckhoff has put in place allows us to create new motion sequences and special effects that were difficult to achieve before,” continues Sébastien Fournier. In fact, his team had reached the limits of what the previous control unit could do – which also meant the limits of what movements could be achieved. The original mechanical structure has been retained, but the five independent control sections are now automatically controlled by five AX5103 servo drives, enabling open and flexible solutions. Just as musicians follow a score, the mechanical units in the stage design also execute changing movements. The speed, duration, and synchronization of these patiences, as they are called, are precisely defined. “Ten movements per patience have been defined for the production, but these could easily be extended to as much as 100,” explains Grégoire Petitbon, who works in sales at Beckhoff in France. This adaptability is greatly appreciated by the stage technology team, as the Opéra Bastille has to cope with an average of 14 different performances per year. As the performances are then exported all over the world, the technical staging must be able to transfer to other theaters or opera houses. Thanks to Beckhoff’s international presence, this is easily achieved.

Customized mechanics

The technicians in the Génie Scénique department at the Opéra national de Paris faced various challenges in adding the patiences and replacing the control system. As they are used to customized solutions, a completely revised approach was taken to the entire system’s historical mechanical design. The team had to rework existing parts or design new ones, adapt the mounting brackets, perform testing, and, if in doubt, start again. This demanding work was carried out entirely in-house, drawing on the team’s extensive experience and expertise. “Everything, from the housing and pulleys to the adapter and spacers, has been tested and reworked to create a link between the old structure and the modern drive technology – and to meet all the requirements we’ll have for moving stage designs now and in the future.”

For Amir Negahdari, an application engineer at Beckhoff France, it is EtherCAT that makes the difference as a high-speed Ethernet system. “The aim is to synchronize the imagery, movement, and lighting in the spirit of the production. With its real-time control, EtherCAT makes this possible in a fast, fluid, and reliable way,” he explains. The Opéra Bastille currently uses five patiences. However, the solution developed with Beckhoff technology and EtherCAT has the ability to control 1,500 patiences simultaneously – all completely safely thanks to Safety over EtherCAT (FsoE).

A close-up of a technical team in front of a server cabinet containing a dense tangle of network cables and equipment.
Behind the scenes: Olivier Harmand, Thibaut Valasse, and Sébastien Fournier from the technical team at the Opéra national de Paris, with Grégoire Petitbon and Amir Negahdari from Beckhoff France (from left to right)

The CX2033 Embedded PC with TwinCAT 3, which is used to integrate the various control processes, offers further technical advantages. Also included are TwinCAT XAR for program execution, TwinCAT XAE for development and programming, and TwinCAT HMI. “All the properties we need, such as motion, the PLC, the HMI, and monitoring, are integrated into the same software environment, which makes our work much easier,” states Sébastien Fournier. “One strength is that the solution can communicate with all communications standards on the market,” adds Amir Negahdari. “This allows us to build bridges – from commonly used fieldbuses to industry-specific protocols such as OSC, DMX, ArtNet, and PSN.” In addition, the Opéra Bastille can use TwinCAT XAE for development and programming purposes without the need to pay an annual license fee. The Opéra Bastille teams no longer have to rely on an external service provider: everything can be done in-house, resulting in significant financial and time savings.

OCT – An ally in confined spaces

As is the case throughout the world of arts productions, Opéra Bastille has limited space for stage technology. In most cases, a separate cable is required to transmit information about position, speed, and temperature so that the patiences can be controlled. Not so with One Cable Technology (OCT) developed by Beckhoff, which combines power and feedback in a standard motor cable. For the Opéra Bastille, this represents significant progress: “It reduces the number of cables in the drag chains and makes the whole thing easier to handle,” says Sébastien Fournier. This becomes all the more important when considering the extensive distances that the Opéra Bastille has to handle: more than 30 meters separate the stage from the control cabinet. Despite this, the OCT cables ensure synchronous real-time communication between the motor and servo drive.

Even though the specifications were drawn up internally, the stage technology department received support from Beckhoff in the form of on-site training for technicians, for example. “We gave them the skills they need to rectify faults quickly themselves,” explains Grégoire Petitbon. In addition, the control system has been designed so that technicians can use the specially developed HMI to easily display, recreate, and save choreographed movement programs, as well as review and analyze warnings and errors. If things come to a stop, however, the team can count on fast support from Beckhoff.

From industry to the world of the stage

Through its culture of innovation, Beckhoff regularly presents new products that highly appeal to the stage technicians at the Opéra Bastille. “We’re benefiting from new developments that are actually made for the industrial world, but contain innovations that also have their place in our opera houses,” summarizes Sébastien Fournier. Although the solution implemented last September is intended to be permanent, it can easily be developed further. “We are currently looking into modernizing the communication interfaces for the sound, lighting, stage design, and video systems,” says Grégoire Petitbon. This could then be implemented as part of the major modernization work planned for 2027 at the Palais Garnier and 2030 at the Opéra Bastille.