Biuras Kaune
Beckhoff Automation OÜ

Karaliaus Mindaugo ave. 38
44307 Kaune, Lietuva

+370 605 42400
info@beckhoff.lt
www.beckhoff.com/lt-lt/

Aug 12, 2020 3:00:00 PM

Part 3: TwinCAT Analytics Workflow – Configurator within the Service Tool

PC-based control and the TwinCAT control software provide a foundation for advanced Industrie 4.0 and Internet of Things architectures in intelligent machines. TwinCAT Analytics is an important element in such an architecture. The product family covers a complete workflow ranging from data acquisition through communication and data historization to data evaluation and representation in web-based dashboards.

In this series of webinars, Pascal Dresselhaus explains the complete TwinCAT Analytics workflow. In addition, the TwinCAT Product Manager presents various application examples. These examples are intended to illustrate, for example, how data analysis capabilities can be used to open up new business areas and generate higher sales revenues. In the four parts of the webinar series, Pascal Dresselhaus will also talk about the high level of application flexibility through the use of IoT technologies and the optimization of support and service processes. Other benefits of TwinCAT Analytics will also be presented, among them time savings in engineering through the automatic generation of PLC code and HMI dashboards. Moreover, attractive licencing packages for the Analytics workflow offering further savings potential will be explained in the webinar.

More about this video

TE1300 | TwinCAT 3 Scope View Professional

TE1300 | TwinCAT 3 Scope View Professional

The TwinCAT 3 Scope View is a software oscilloscope for the graphic representation of signal curves in different chart types. These could be, for example, YT, XY, bar or digital charts. The Scope View Professional extends the Scope View Base version supplied with TwinCAT 3 XAE by additional functionalities. The field of application refers to processes that are to be tracked and monitored over a longer period of time.

TE3500 | TwinCAT 3 Analytics Workbench

TE3500 | TwinCAT 3 Analytics Workbench

The TwinCAT 3 Analytics Workbench is a TwinCAT 3 engineering product for creating continuous data analyses. The data can come from various applications such as machines, buildings, or energy systems, for example. The configuration of the workbench is integrated into Microsoft Visual Studio and is designed as a graphical user interface. Many algorithms for configuring the analysis are available in a toolbox:

TE3520 | TwinCAT 3 Analytics Service Tool

TE3520 | TwinCAT 3 Analytics Service Tool

The TwinCAT 3 Analytics Service Tool is a TwinCAT 3 engineering product for the evaluation of live and/or historicized data. The data can come from various applications such as machines, buildings, or energy systems, for example. The configuration of the Service Tool is integrated into Microsoft Visual Studio and is designed as a graphical user interface. Many algorithms for configuring the analysis are available in a toolbox: