DetachFixClose

Nov 24, 2022

Cabinet dome for industrial WLAN and mobile network components

The cabinet dome has been specially developed for industrial WLAN and mobile network components. The material used is characterized by high stability and impact resistance, and is optimally suited for radio applications as a result of its nature.

More about this video

CU8210-M002-0100 | Cabinet dome for industrial WLAN and mobile network components

CU8210-M002-0100 | Cabinet dome for industrial WLAN and mobile network components

The cabinet dome has been specially developed for industrial WLAN and mobile network components. The material used is characterized by high stability and impact resistance, and is optimally suited for radio applications as a result of its nature.

CU8210-M001-01x0 | Cabinet dome for industrial WLAN and mobile network components

CU8210-M001-01x0 | Cabinet dome for industrial WLAN and mobile network components

The cabinet dome is designed for industrial WLAN and mobile communication components, and meets IP66 requirements when properly mounted to a control cabinet. The components inside the cabinet dome are fully protected against physical contact, dust, and splash water. The material used is characterized by high stability and impact resistance, and its properties make it perfectly suitable for radio applications.

CU8210-D001-0101 | WLAN USB stick for USA, Canada

CU8210-D001-0101 | WLAN USB stick for USA, Canada

The WLAN sticks from the CU8210-D001 series can be used as high-performance wireless clients and enable encrypted data at rates of up to 433.3 Mbit/s. With the help of the Beckhoff Virtual WLAN Access Point software tool, the sticks can be configured via Wi-Fi Direct to serve as Virtual Access Points on Industrial PCs, which opens up new fields of applications. The WLAN sticks are fully compatible with all previous and current WLAN standards. Thanks to their downward compatibility, the sticks also can easily be connected to older WLAN infrastructures. The WLAN sticks support 20 MHz, 40 MHz and 80 MHz transmission bandwidths.

CU8210-D001-0102 | WLAN USB stick for Europe, Russia, South Africa, Israel, Korea, Taiwan, China, Japan, Australia, New Zealand, India

CU8210-D001-0102 | WLAN USB stick for Europe, Russia, South Africa, Israel, Korea, Taiwan, China, Japan, Australia, New Zealand, India

The WLAN sticks from the CU8210-D001 series can be used as high-performance wireless clients and enable encrypted data at rates of up to 433.3 Mbit/s. With the help of the Beckhoff Virtual WLAN Access Point software tool, the sticks can be configured via Wi-Fi Direct to serve as Virtual Access Points on Industrial PCs, which opens up new fields of applications. The WLAN sticks are fully compatible with all previous and current WLAN standards. Thanks to their downward compatibility, the sticks also can easily be connected to older WLAN infrastructures. The WLAN sticks support 20 MHz, 40 MHz and 80 MHz transmission bandwidths.

CU8210-D001-0200 | WLAN USB stick for Arm®-based devices with Windows CE, for Europe, China

CU8210-D001-0200 | WLAN USB stick for Arm®-based devices with Windows CE, for Europe, China

With the CU8210-D001-0200 WLAN stick, Beckhoff Industrial PCs can be equipped with a WLAN module and operated under Windows CE in client mode.

CU8210-D004-0200 | LTE USB stick for USA, Canada, Europe, Taiwan, Australia, New Zealand

CU8210-D004-0200 | LTE USB stick for USA, Canada, Europe, Taiwan, Australia, New Zealand

The LTE USB stick with a GSM/UMTS/LTE modem can dial into a mobile communication network via a common SIM card. The stick can be used to retrofit Industrial PCs with mobile communication if the need arises. This means there are virtually no limits to connectivity to databases and cloud systems. Also, an Internet connection can be set up even in less populated areas, given sufficient cellular coverage. The stick uses the fourth generation (4G) cellular network technology, has a slot for a SIM card, an additional slot for a microSD card and is supplied with power via the USB interface.