解除修正閉じる

Dec 16, 2013

Google Glass: TwinCAT automation software

Google Glass can be integrated in the control technology via the TwinCAT automation software. In the technology example shown the glasses communicate with a web server that supplies the status of the TwinCAT-controlled machine. The Google glasses receive and display this machine status in the form of signal values or error messages and refer if necessary to the precise error location. The acknowledgment and resetting of the machine status is also possible directly on the glasses.