Beckhoff’s TwinCAT 3 CoAgent brings AI-supported assistance directly into machine operation for the first time: in addition to the proven CoAgent for Engineering, which supports control programmers with precise code suggestions, optimizations, and automatic documentation, the new CoAgent for Operations module enables agentic technology to be used live on the system itself. Watch the video to discover exactly how this AI assistant works – from development to the machine.
More about this video
TE1700 | TwinCAT 3 CoAgent for Engineering
TwinCAT 3 CoAgent for Engineering is the intelligent AI assistant that provides efficient support for PLC development, I/O configuration, and human-machine interface creation. Requirements can be formulated in normal language and TwinCAT CoAgent for Engineering suggests suitable code and configurations, taking existing project structures into account. Flexible mode selection enables custom support based on the task at hand. In addition, TwinCAT CoAgent for Engineering offers direct access to the documentation in the Beckhoff Information System and provides context-related recommendations for accelerated high-quality project implementation.
TF1700 | TwinCAT 3 CoAgent for Operations
TwinCAT 3 CoAgent for Operations is the intelligent AI assistant that provides efficient support in machine operation, maintenance, and system diagnostics. Operating and maintenance tasks are described in natural language. The CoAgent then provides specific recommendations for action, diagnostics, or direct system commands based on the current machine and process data.