With the new Build 4024, Beckhoff is integrating a large number of new features into the TwinCAT 3.1 automation software. Dr. Henning Mersch, Product Manager TwinCAT, presents the new items for programming in C++ in this 30-minute webinar. Learn more about:
- exchange of the C++ program version at runtime
- application for Matlab-Simulink modules
- management of different program versions in the engineering and goal
- TwinCAT Module Executables (TMX) with TwinCAT OEM certificates.
The webinar is aimed at technically oriented users.
More about this video
TC1210 | TwinCAT 3 PLC/C++
Based on the TwinCAT 3 PLC TC1200, TC1210 offers the additional option of using C++ modules in the runtime parallel to the PLC through TC1300 TwinCAT 3 C++.
TC1220 | TwinCAT 3 PLC/C++/MATLAB® and Simulink®
Based on TC1210 TwinCAT 3 PLC/C++ and through TC1320 TwinCAT 3 C++/MATLAB® and Simulink®, TC1220 additionally offers the possibility to use modules in MATLAB® and Simulink®. MATLAB® and Simulink® is a widely used development environment in the scientific field and is used, among other things, for the description of dynamic systems. From this environment, it is possible to generate C++ code that implements the behavior described. TwinCAT 3 runtime modules can be generated using TE140x products.
TC1300 | TwinCAT 3 C++
C++ is one of the most widely used programming languages, especially when it comes to hardware-oriented programming. The continual further development of C++, which is reflected in the further development of the compiler and tooling over the last few decades, is driven forward by an active developer community.
TC1320 | TwinCAT 3 C++/MATLAB® and Simulink®
MATLAB® and Simulink® is a widely used development environment in the scientific field and is used, among other things, for the description of dynamic systems. From this environment, it is possible to generate C++ code that implements the behavior described. TwinCAT 3 runtime modules can be generated using TE140x products.