Oficina central México
Beckhoff Automation, S.A. de C.V.

Boulevard Manuel Ávila Camacho 2610, Torre B, Piso 9, Colonia Valle de los Pinos, Tlalnepantla de Baz
Estado de México CP 54040, México

+52 55 75998058
mexico@beckhoff.com
www.beckhoff.com/es-mx/

Nov 25, 2025

Physical AI with TwinCAT CoAgent for Operations

An industrial robot programmed by voice command – made possible by TwinCAT CoAgent for Operations. TwinCAT CoAgent provides various agents that use the Model Context Protocol (MCP) to enable users to interact directly with the machine using questions or commands. This AI agent translates natural language into executable processes, orchestrates control, planning, and diagnostics in real time, ensures secure monitoring and efficient troubleshooting – and even plays chess on the side.

More about this video

ATRO | Automation Technology for Robotics

ATRO | Automation Technology for Robotics

The ATRO system offers a unique, modular, and flexible industrial robot system that is fully integrated into the Beckhoff automation system.

TwinCAT CoAgent

TwinCAT CoAgent

TwinCAT CoAgent offers comprehensive, intelligent support and combines state-of-the-art generative AI models with custom-developed AI agents.

TE1700 | TwinCAT 3 CoAgent for Engineering

TE1700 | TwinCAT 3 CoAgent for Engineering

TwinCAT 3 CoAgent for Engineering is the intelligent AI assistant that provides efficient support for PLC development, I/O configuration, and human-machine interface creation. Requirements can be formulated in normal language and TwinCAT CoAgent for Engineering suggests suitable code and configurations, taking existing project structures into account. Flexible mode selection enables custom support based on the task at hand. In addition, TwinCAT CoAgent for Engineering offers direct access to the documentation in the Beckhoff Information System and provides context-related recommendations for accelerated high-quality project implementation.

TF1700 | TwinCAT 3 CoAgent for Operations

TF1700 | TwinCAT 3 CoAgent for Operations

TwinCAT 3 CoAgent for Operations is the intelligent AI assistant that provides efficient support in machine operation, maintenance, and system diagnostics. Operating and maintenance tasks are described in natural language. The CoAgent then provides specific recommendations for action, diagnostics, or direct system commands based on the current machine and process data.