Oct 1, 2026

“TwinCAT is at the heart of our engineering workflow”

Interview with Peter Quinlan of 38Ten and Mark Ager of XM Automation on the benefits of PC-based control in stage technology

As electromechanical and hydraulic systems for live productions become increasingly complex, there is a need for customized automation solutions that prioritize precision, system flexibility, and the highest safety standards. In this interview, Peter Quinlan, managing director at 38Ten, and Mark Ager, director at XM Automation, explain why PC-based control and TwinCAT from Beckhoff are the right platform for sophisticated stage architectures.

Peter Quinlan: “To avoid design errors and increase efficiency, we routinely rely on TwinCAT for motion design.”
Peter Quinlan: “To avoid design errors and increase efficiency, we routinely rely on TwinCAT for motion design.”

38Ten specializes in automation solutions for the entertainment industry. What technological requirements shape your daily work?

Peter Quinlan: We focus on the design and implementation of complex electromechanical and hydraulic systems for live productions, events, theater, and film and television. Our service portfolio covers the entire life cycle – from basic system design and detailed engineering through to on-site support. The greatest technological challenge lies in translating creative concepts into safe, precise, and standards-compliant motion control applications that ensure absolute reliability under the harsh conditions of live operation. In doing so, we rely not only on Beckhoff control technology, but also on its drives, safety systems, and I/Os. It is precisely the huge variety of fieldbus options, standards, and physical interfaces that can be supported by EtherCAT Terminals that is crucial to the flexibility of our system topologies.

XM Automation focuses on open control concepts for stage automation. What are your key areas of technological focus and how do your areas of expertise complement those of 38Ten in joint projects?

Mark Ager: Our industry has traditionally been dominated by closed, proprietary systems. This often makes system expansions or retrofits inflexible and cost-intensive for end users. Our strategic goal is to break down the so-called walled gardens of traditional providers and make control systems interoperable. As our core product, we are developing the XMove front end in combination with an open communication protocol and open-source Beckhoff PLC code. This is where the perfect technological synergy with 38Ten comes into play: While XM Automation provides the modular software architecture and the graphical user interface as the higher-level front end, 38Ten is responsible for the detailed physical engineering of the complex electromechanical and hydraulic machines. By consistently using PC-based control, 38Ten is able to integrate our interfaces natively into the system control system. End users therefore benefit from a highly flexible systems toolkit – a genuine pick-and-mix approach. They are not forced into a single-vendor ecosystem; instead, they can combine mechanical engineering and the software front end in a way that is manufacturer-independent, scalable, and future-proof.

The design of mechatronic systems requires a high degree of precision as early as the concept phase. What role does automation software play in this context?

Peter Quinlan: In the early stages of a project, the primary focus is on precisely sizing the drive technology and motors for the specific load and motion conditions. A consistent software environment is essential here to avoid design errors and increase efficiency. That’s why we routinely rely on TwinCAT for motion design. Even I regularly use the software on my laptop for these initial calculations as part of my daily work, even though I’m no longer as heavily involved in the subsequent code implementation as I used to be. The tool provides us with precise data for drive sizing and, in doing so, lays the foundation for a reliable system architecture.

Mark Ager: “PC-based control allows interfaces to be integrated natively into the system control system – enabling end users to benefit from a highly flexible systems toolkit.”
Mark Ager: “PC-based control allows interfaces to be integrated natively into the system control system – enabling end users to benefit from a highly flexible systems toolkit.”

So TwinCAT is an important part of developers’ daily work?

Peter Quinlan: It certainly is. TwinCAT is at the heart of our engineering workflow. The software team spends every working day in the TwinCAT XAE development environment. We don’t work with fragmented, isolated solutions; instead, we have a central development platform for PLCs, motion control, and functional safety. Deep integration into our technology stack significantly speeds up programming and reduces interface complexity.

XM Automation and 38Ten carry out many projects on an international scale. How does Beckhoff’s system architecture support such cross-border engineering processes?

Mark Ager: Our collaboration requires a seamless technological foundation. A standardized technology stack is invaluable for working across continents. Since both companies rely on PC-based control and TwinCAT as their engineering environment, software modules, safety concepts, and drive configurations can be exchanged seamlessly. This consistency drastically reduces friction losses during commissioning and ensures a consistently high level of quality. This ultimately results in reliable, future-proof, and customized automation solutions for stage technology, which we also implement under the Open Automation joint brand.

What does the future technology roadmap look like and what is the long-term outlook for the strategic partnership with Beckhoff?

Peter Quinlan: We are constantly evaluating new automation technologies to push the boundaries of what is physically possible in live entertainment. Our partnership with Beckhoff provides us with the necessary scalability and ensures the security of our technology investments. Because we receive genuine support at the engineering level, we are able to implement even the most sophisticated motion control tasks in a manner that ensures process reliability, complies with standards, and offers economic efficiency.