DetachFixClose
xts-nct-gesamtsystem-stage-lowres

Apr 27, 2023

How XTS movers can replace robots

XTS with NCT: Linear transport system as a highly flexible multi-robot system

The XTS linear transport system from Beckhoff has already proven to be an innovation factor in thousands of machines, and the ongoing expansion of its range of functions offers plenty of market potential for the future. A prime example here is No Cable Technology (NCT), which provides contactless energy transfer and synchronous real-time data communication directly on the XTS movers. This allows the movers to perform a variety of different robot functions via end effectors. Furthermore, the ability to have a large number of movers on an XTS enables a flexible multi-robot system that increases area productivity many times over by executing process steps in parallel.

Thomas Beckhoff, Product Manager XTS, Beckhoff Automation
Thomas Beckhoff, Product Manager XTS, Beckhoff Automation

XTS is a linear transport system in which a large number of movers move independently of each other along a track. The movers offer a host of functionalities, including forming groups and synchronizing to other process sequences. The track is made up of motor modules based on a modular principle, and can be open or closed to facilitate the implementation of application-specific system layouts. A closed travel path enables an increase in productivity, as the movers do not have to return to the starting point on the production line empty.

No Cable Technology as an extension supports the use of a wide variety of end effectors without reducing the high dynamics and flexibility of the XTS solution. End effectors mounted on the mover, such as standard actuators or sensors, are used to perform various process steps during linear travel. In the packaging sector, for example, almost all conveyor, sorting, robotic, or material handling systems for the infeed or manufacturing process can benefit from this technology. This allows new breakthrough solutions to be created that enable sophisticated product and material handling in highly automated systems. In addition, the XTS and NTC reduce the required installation space many times over compared to conventional robotic systems, allowing significantly more functionality to be accommodated in less space.

Virtually unlimited application possibilities

As one of many examples, motion sequences can be implemented directly on the mover for performing tasks such as rotating and aligning a product for scanning a barcode or running quality checks. Electromotive grippers, magnetic grippers, or vacuum cups on the movers can pick up, transfer, and deposit products on the fly, making the movers mobile material flow systems.

The end effector on the XTS mover with NCT aligns the product to facilitate barcode scanning or quality inspections.
The end effector on the XTS mover with NCT aligns the product to facilitate barcode scanning or quality inspections.

Countless applications stand to benefit from the use of a multi-gripper system such as this. In a meal kit filling application, for example, various electromechanical or vacuum grippers would collect the necessary ingredients to assemble a complete menu. The movers would pick up the ingredients from predefined stations and place them at individual product locations, facilitating an exclusively software-based format changeover up to production with a lot size of one. Thanks to the traceability of the XTS, every ingredient could be tracked seamlessly from picking to order labeling and supplier pickup. Pharmaceuticals are another similarly obvious use case. Here, the appropriate end effector could rotate a container so that it can be sealed or validated.

Fully compatible function extension

Since the XTS elements with NCT are fully compatible with the standard system, NCT can be integrated into existing XTS applications. The continued use of existing system components not only cuts down on implementation time, but also saves resources. Furthermore, the complete integration into the XTS modular system offers the advantage that no additional components are required apart from the end effectors used. The end effectors on the movers are also controlled via the central TwinCAT automation software, allowing all processes in TwinCAT to be coordinated with microsecond precision, and the engineering effort to be reduced to a minimum.