Văn Phòng Đại Diện tại Việt Nam

#29.05, Tòa nhà Pearl Plaza, 561A, Đường Điện Biên Phủ
Phường 25, Quận Bình Thạnh
Thành Phố Hồ Chí Minh, Việt Nam

+84 28 7300-2439
info@beckhoff.com.vn
www.beckhoff.com/vi-vn/

Oct 20, 2021 5:30:00 PM

TwinSAFE Tutorial 17: TwinSAFE Loader Customizing

In this tutorial we will show you how to customize a new safety project in the TwinSAFE Loader.

More about this video

TE9200 | TwinSAFE Loader/User

TE9200 | TwinSAFE Loader/User

With the TwinSAFE Loader, Beckhoff Engineering provides a command line tool that allows the download and customizing of safety projects during runtime. This means that the use of the TwinCAT 3 development environment is not mandatory.

TE5950 | TwinCAT 3 Drive Manager 2

TE5950 | TwinCAT 3 Drive Manager 2

The TwinCAT 3 Drive Manager 2 is used for commissioning the AX8000 multi-axis servo system, AX5000 digital compact servo drive, AMP8000 distributed servo drive system, AMI8100 integrated servo drives or the EL72xx, EL74xx, EL70x7, ELM72xx, EP72xx and EJ72xx I/O components. It is optionally available as an integrated version in the TwinCAT automation platform or an update version independently of TwinCAT. The TwinCAT 3 Drive Manager 2 is integrated into a TwinCAT solution as a project and enables a separate assessment of power supply modules, axis modules and axis channels.