Oct 14, 2026

“Kinetics, light, and interaction in real time”

Interview with Martin Munder, MKTe, on PC-based control for kinetic art and technical exhibits

MKT engineering (MKTe) develops and builds kinetic installations, technical exhibits, prototypes, and custom-made mechatronic structures for museums, visitor centers, brand experiences, architectural projects, and leisure attractions: these are sophisticated applications that often feature hundreds of synchronized drives and are designed for safe, continuous operation. Martin Munder, CTO of MKTe, on creative engineering, interactive experiences, and the question of where the limits lie for kinetic systems today.

“Together with Beckhoff, we continually push the boundaries of what’s technically feasible and think one step ahead when faced with new requirements.” – Martin Munder, CTO, MKTe
“Together with Beckhoff, we continually push the boundaries of what’s technically feasible and think one step ahead when faced with new requirements.” – Martin Munder, CTO, MKTe

Your motto is ‘Engineering Magic’. What does this entail technically?

Our strength is in combining creative engineering with industrial reliability. We support projects from the initial feasibility study through design, control system development, and manufacturing to worldwide installation and maintenance. Many of our systems consist of hundreds of synchronized drives and are designed for safe, continuous operation. Our customers benefit from a high degree of vertical integration, extensive expertise in control systems, and the ability to implement the necessary technology even for ideas that seem impossible.

What does this mean in terms of modern automation technology?

For a number of years now, we’ve been seeing a strong trend toward interactive and data-driven worlds of experience. Today’s customers expect not just movement, but a combination of kinetics, light, media, and interaction in real time. At the same time, the demands for reliability, security, remote maintenance, and scalability are increasing. MKTe has responded to this trend by continuously expanding our expertise in the areas of control systems, software development, data integration, and remote service. In addition, virtual prototypes are used early in the engineering process to minimize technical risks and reduce development times.

How did the collaboration with Beckhoff as an automation partner come about?

When working on our early kinetic installations, we were faced with the challenge of finding a solution to control large numbers of drives that was both precise and synchronized. This is when we became aware of Beckhoff and PC-based control. The automation technology from Beckhoff has quickly proven to be a high-performance solution, particularly in the context of complex motion sequences, distributed systems, and sophisticated real-time applications. We’ve been working together closely for over ten years now. Together, we continually push the boundaries of what’s technically feasible, make the most of existing possibilities, and think one step ahead when faced with new requirements. In addition to the technological platform, we value personal and direct engagement. As a result, our long-standing collaboration has evolved into a trusting partnership that forms an integral part of many of our projects.

For the ‘Resonanzen’ project, MKTe developed all the control and drive technology for 900 individually activated motion elements on behalf of its partner agency ART+COM.
For the ‘Resonanzen’ project, MKTe developed all the control and drive technology for 900 individually activated motion elements on behalf of its partner agency ART+COM.

Which specific technical attributes won you over?

From our perspective, Beckhoff is renowned above all for its combination of openness, flexibility, and performance. Added to this are the seamless integration of control, motion, and safety systems, as well as visualization, powerful engineering tools, and high scalability. The same technological basis can be used for everything from a single prototype to a large-scale kinetic installation. Depending on the project, we use high-performance industrial or embedded PCs with TwinCAT 3 and EtherCAT as our end-to-end communication platform. For servo axes, we use servo drives from the AX series, for example. We use EtherCAT Terminals from the EL series to integrate stepper motor axes as well as digital, analog, and safety-oriented signals. Based on risk assessments, we use TwinSAFE to implement safety-oriented functions up to performance level e. A particular advantage for us is the high degree of flexibility in relation to I/O and interfaces. This allows us to combine our solutions with higher-level control systems as well as building and media technology systems. Especially in the field of international museum and exhibition design, we come across a wide range of different infrastructures, each of which requires us to establish an appropriate level of communication.

MKTe’s large-scale kinetic installations are incredibly spectacular.

As mentioned at the start, several hundred motion elements often work together here continuously in precisely choreographed sequences. To achieve this, we combine mechanics, electronics, software, lighting, and architecture to create a complete experience. The Beckhoff control system handles the synchronization and coordination of all motion sequences. A current example is the ‘Resonanzen’ project, which we’re implementing on behalf of our partner agency ART+COM for the Japanese construction company Ichijo, and for which we’ve developed all the control and drive technology for 900 individually activated motion elements.

What technical challenges is your company facing as it looks to the future?

Demand for immersive experiences is growing all the time. Systems are becoming increasingly complex, yet they’re expected to be energy-efficient, low-maintenance, and economical. Another challenge is the increasing integration of all technical systems. For MKTe, this means continuing to expand our expertise accordingly. At the same time, we want to keep pushing the boundaries of what’s technically possible with kinetic systems.

What does the partnership with Beckhoff mean for your future projects?

We’re constantly working on new concepts for interactive and adaptive installations that respond to the environment or to user interaction. To do this, we need a powerful, future-proof automation platform. Our experience with Beckhoff automation technology shows that its openness and scalability are an excellent fit for our project business. This collaboration makes it possible to efficiently transform creative ideas into robust, sustainable solutions. Ultimately, for us, Beckhoff is much more than just a supplier of components: PC-based control represents a key foundation for implementing complex mechatronic systems.