Văn Phòng Đại Diện tại Việt Nam

#29.05, Tòa nhà Pearl Plaza, 561A, Đường Điện Biên Phủ
Phường 25, Quận Bình Thạnh
Thành Phố Hồ Chí Minh, Việt Nam

+84 28 7300-2439
info@beckhoff.com.vn
www.beckhoff.com/vi-vn/

Mar 2, 2021 3:30:00 PM

TwinCAT Bode Plot: Optimization of drives in machine applications

The TwinCAT 3 Bode Plot Base is the ideal tool in the TwinCAT Engineering for the optimization of drives in machine applications. It displays frequency response and phase in graphic form and thus indicates possible optimizations of the axis properties. Several plots can be simulated and at the same time displayed.

In this 30-minute webinar, Daniel Viermann from the Application and Support Dept. for Drive Technology demonstrates the use and subsequently the interpretation of the Bode Plot. After that, he will show how a perfect adjustment of the drive for the respective mechanism can be achieved through the use of filters.